Go to online shop
electronic assemblies in a wave soldering machine

Soldering Technology in Manufacturing: From Manual Soldering Stations to Reflow Systems

Hand soldering, selective soldering, wave soldering, or reflow soldering: In practice, several soldering processes are often used in parallel today – within the same company, sometimes even on the same line. This is because what works perfectly in prototype construction can quickly lead to bottlenecks in series production. In addition, highly automated processes are not always the best solution for every assembly. This article provides a structured overview of common soldering techniques and offers decision-making aids for selection in practice.

Posted by Roberto Bellandi | | 6 min read

Why soldering technology is so diverse today

There is a simple reason why there are so many soldering processes today: the requirements in manufacturing have changed significantly.

  • Components are getting smaller
  • Assemblies are becoming more complex
  • Quality requirements are increasing
  • Cost and time pressures are increasing
  • Flexibility is a must

Learn more about the assembly of electronic components

Manual soldering stations: the classic in manufacturing

Manual soldering stations are often the first point of contact with professional soldering technology – and they are not disappearing from modern manufacturing facilities. On the contrary: Manual soldering stations remain relevant because there are always tasks that are difficult to automate.

View soldering products

Typical areas of application for manual soldering

  • Prototype construction and development
  • Rework and repair
  • THT components in small series
  • Cable assembly
  • Special assemblies, variant production, small quantities

What makes a good manual soldering station?

A good manual soldering station consists of more than just a soldering iron and solder. The key is a setup that makes quality reproducible while remaining efficient.

Important components:

Would you like to learn more about ESD protection in the workplace? We have summarized the most important information for you: Read the article

Manual soldering: Advantages and limitations

Manual soldering is ideal for beginners. However, stable series processes often require supplementary or automated procedures.

Advantages

  • Very flexible, quick to use
  • Low investment costs
  • Ideal for individual pieces and adjustments

Disadvantages

  • Highly dependent on experience and daily form
  • Quality fluctuates without clear process specifications
  • Quickly becomes inefficient as quantities increase
  • Risk of thermal overload (components/PCB)

Selective soldering and wave soldering: The bridge between manual work and automation

As quantities increase, a purely manual soldering process is often no longer sufficient. The challenge: higher throughput and consistent quality without losing flexibility. This is where processes such as selective and wave soldering come into play. In many manufacturing operations, they represent the next stage of expansion, as they offer more stable processes and more predictable cycle times with less manual work.

Wave soldering: fast, robust, but less flexible

Wave soldering is an automated soldering process that is mainly used for THT components (through-hole technology). In this process, the printed circuit board runs over a wave of liquid solder. This solder wave wets the through-hole pins and pads on the underside, while the solder also rises into the through-hole via capillary action.

Strengths

  • High speed
  • Proven technology for series production
  • Economical for suitable assemblies

Challenges

  • Less suitable for complex mixed-tech assemblies
  • Masking/covering may be necessary
  • Solder bridges and shadow effects possibl

Wave soldering works particularly well when …

  • many THT pins need to be soldered.
  • the assemblies are standardized.
  • the process is to run stably over long series.

Selective soldering: automated – but targeted

In selective soldering, only certain solder joints on a printed circuit board are soldered, usually THT pins or individual areas of an assembly. In contrast to wave soldering, the solder is therefore only applied where it is needed.

Strengths

  • Good repeatability
  • Often less thermal stress
  • Ideal for more complex assemblies

Challenges

  • Programming/setup requires expertise
  • Process window must be clearly defined
  • Not every geometry is trivial (distances, shadowing)

Selective soldering works particularly well when …

  • only certain areas need to be soldered.
  • the assembly has sensitive SMD zones.
  • mixed technology is used.

Reflow soldering: Standard in SMD series production

When it comes to modern electronics manufacturing, there is hardly any way around reflow soldering, especially for SMD assembly.

What is reflow?

Reflow means that the solder is not applied directly with a tip, but as solder paste  printed onto pads. The components are then placed and heated in a controlled manner in the oven until the paste melts and a solder joint is formed. The process is so widespread because it is highly automatable, enables high packing densities, and delivers reproducible quality.

Good to know

How does a reflow oven work?

A reflow oven heats assembled circuit boards in a controlled manner in several temperature zones so that the solder paste melts and stable solder joints are formed on the SMD components

  1. Preheating
  2. Soak/temperature equalization
  3. Reflow/peak zone (solder melts)
  4. Cooling (solder joint solidifies)

Good to know: Reflow soldering systems are usually the heart of an SMD production line. After the assembly has been heated in the reflow oven, optical inspections, for example by AOI, follow depending on the quality requirements, and, if necessary, rework at the manual soldering station.

Comparison: Which soldering technique is suitable for which application?

The appropriate soldering technique is usually determined by a balance between technical requirements and cost-effectiveness:

Quantity and throughput

  • Manual soldering: ideal for single pieces, small series, rework
  • Selective/wave: good for medium to large series (THT/mixed)
  • Reflow: strong for series production with SMD

Process stability and repeatability

  • Manual soldering: varies depending on the operator
  • Selective/wave: stable with a clean setup
  • Reflow: very stable with good profile and material management

Investment costs

  • Manual soldering: low
  • Selective/wave: medium to high
  • Reflow: high (line + peripherals), but scalable

Flexibility with variants

  • Hand soldering: very high
  • Selective: high (programmable)
  • Wave soldering: rather low
  • Reflow: high, but with setup effort (stencils, profiles)

Typical fault patterns

  • Manual soldering: overheating, cold solder joints, too much/too little solder
  • Wave: bridges, shadows, solder beads
  • Selective: incomplete wetting with difficult geometry
  • Reflow: tombstoning, voids, head-in-pillow

Deciding: Questions to ask yourself

Depending on the manufacturing environment, different approaches can lead to the optimal process. The following key questions will help you make your choice:

  • What assemblies do you manufacture (SMD-only, THT-only, or mixed technology)?
  • What quantities are realistic (today and in 12 months)?
  • Where are the current bottlenecks?
  • How important are documentation and traceability?
  • How much rework is acceptable?
Good to know

Rule of thumb for selection

  • Hand soldering: when flexibility is more important than cycle time
  • Selective soldering: when reproducible THT solder joints in mixed tech are required
  • Wave soldering: when the focus is on robust series processes with suitable assemblies
  • Reflow: when SMD series production, miniaturization, and automation dominate

Soldering technology as a process decision

In electronics manufacturing, soldering technology is rarely a single process that covers everything. Manual soldering remains important, for example for prototypes, rework, or small quantities. As soon as throughput and repeatability become more important, semi-automated processes become a logical addition.

The decisive factor is not so much the best technology, but rather the right process for your own manufacturing reality. Those who understand soldering technology as a modular principle make more informed decisions – not only technically, but also economically.

Posted by Roberto Bellandi, Roberto Bellandi is one of the product managers at Bürklin Elektronik. He is responsible for measurement technology, tools and workshop supplies, soldering technology, enclosures as well as chemical products. Roberto joined Bürklin Elektronik in 2017 and has over 25 years of experience as a product manager in the electronics industry. Previously, he worked for various electronics distributors. He is an expert in his fields and is interested in all topics related to renewable energies.