Wire-wrapping tools

Wire-wrapping tools

For wire-wrap technology special tools are required. This electrical connection technology uses a high contact pressure, which establishes an oxide-free and gas-tight contact point. Wire is wrapped around a sharp-edged pin with the help of a wire wrap gun. The wire wrap gun automatically strips the wire, wraps it around the pin and separates the wire. There are also manual wire wrap tools available, so-called hand mandrels, which are used for winding or unwinding. The advantage of these tools is that they can be used anywhere and without electricity. Wire-wrap technology and wire-wrap tools are used in the construction of prototypes, for example.

Items per page: 20