Receptacles and insulating sleeves

Receptacles and insulating sleeves

Cables can be connected to electrical contact points using receptacles. The receptacle contact is made of conductive metal. The cable is inserted into one end of the receptacle and is clamped using crimp pliers. The matching contact spade is inserted into the other end of the receptacle. Depending on the application, insulating sleeves are provided in various colours, to protect the receptacle. The advantage of receptacles is that they allow an electrical contact to be created quickly and easily. Receptacles are used for instance for the cabling of cars.

Items per page: 20