Micrometers

Micrometers

Small lengths are measured with micrometers. They are also referred to as a precision micrometers. The part to be measured is located inside the bracket between two measurement surfaces. A measurement is performed by turning an adjusting screw as far as it will go so that the two measuring surfaces touch the test piece. The distance between the two measurement surfaces can be read on an analogue or digital scale. Since micrometers are made of steel, and this material is thermally conductive, there is also special hand temperature protection made of plastic, so that the body heat does not distort the measurement result. Micrometers are used for measuring the dimensions of mechanical components, for example.

Items per page: 20