Low-voltage halogen lamps

Low-voltage halogen lamps

Our ranges of low-voltage halogen lamps require a voltage of 12 volts for operation. Therefore, the use of a transformer is necessary. Compared to conventional lamps, energy savings of up to 50% are possible. In addition, the lifetime increases by several factors. However, it must not be dispensed with natural light, which can also be dimmed steplessly. Optimum directional light, which can be further intensified by a reflector, is an advantage when illuminating objects, e.g., in display cabinets or shop windows, but also in public spaces. In addition, low-voltage halogen lamps provide excellent lighting when working, reading or cooking.