Hot air stations

Hot air stations

Unlike soldering irons, hot air systems work without any contact. A stream of hot air is produced to heat up the material. The most important settings on the station are the temperature and the strength of the air stream. They are mainly used for soldering and desoldering SMD components, as they work in a particularly precise way. Removed parts can be reused using this method. Wired elements such as plugs and sockets can be modified or shrink film can be applied to wires and cables.

Items per page: 20