Film resistors

Film resistors

Metal film resistors promise high long-term stability, quick response times, a long working life and very high precision. These are achieved by use of a special production process. The film in the resistor consists of a nickel-chromium alloy, which is applied in the micrometre range on to a ceramic base body. This means the resistor is exceptionally precise, even at high temperatures, which property can be traced back to the low coefficients of thermal expansion. Film resistors are used for instance in power modules, frequency converters and switch-mode power supplies. Their precision renders them particularly suitable for medical technology, aerospace and military applications.

Items per page: 20