Feeler gauges

Feeler gauges

These types of gauges are used for checking gap dimensions. They consist of a set of different metal strips that can be turned out like a fan. The thickness is engraved on the individual metal strips. For gap widths which cannot be determined using other measuring tools, it is sufficient to push the strongest-possible metal strip into the gap. The gap width can then be easily read on the plate thickness. Feeler gauges are used to check and adjust the distance between electrodes, for example.

Items per page: 20