Cutting pliers

Cutting pliers

This type of pliers is used to cut or pinch off material. They have cutting edges positioned in the centre of the jaw or on the side, for different requirements. The cutting edges can be bevelled on both sides or just one side and in different sizes. For very strong wires a cutting edge with large bevels is required. Centre cutters are another type of cutting edge, where a relatively small amount of force is needed compared with long side cutters. Hose and pipe cutters, which are equipped with a knife, also belong to the cutting pliers category.

Items per page: 20