Centre punches

Centre punches

Centre punches are used to make an indent in metal or plastic prior to drilling a hole. The centre punch - which is a type of chisel - is placed at the drilling location and by striking the centre punch a small indent is made in the material. This indent is the marking point for the tip of the drill. and prevents the drill bit from slipping. This allows the bore hole to be drilled in the exact location. Centre punches are used in the field of electronics, especially for assembly work.

Items per page: 20