Skip to content Skip to navigation menu
Outlet Strips

Outlet Strips

What is a power strip?

Power strips are extension leads (UK) or cords (US with a socket or sockets that allow you to supply power to several devices in one location. Power strips are available in many different cable lengths and designs. In addition, multiple sockets must have a certain degree of safety in order not to trigger a short circuit. Depending on the application you need one with different properties.

Bürklin Elektronik also offers the following options for power strips:

  • Socket strip with switch: So that devices in standby mode do not draw more power than they already do, you can simply switch them off with the switch.
  • Power strip with USB: In the digital age of smartphones, tablets and the like, you can simply connect your cable to the USB socket and charge it from there
  • Power strip with master-slave function: One main device (master) and several auxiliary devices (slave) are connected to the strip
     If, for example, the main unit is switched off, the ancillary units also switch off automatically This is how you can also save energy
  • Power strip with surge protection: In order to avoid overvoltage surges that affect sensitive electronic devices, surge protection is very important.
  • Earthed power strip (Schuko): Schuko is the abbreviation for the standard socket used in many European countries (CEE 7/7). Schuko power strips ensure that hazardous voltages are grounded when the plug is pulled out

What are the benefits of a power strip with overvoltage protection?

In the multiple socket power strip there is a built-in overvoltage protection which ensures that all connected devices are protected against excessively high electrical voltages (e.g. by lightning). So the devices connected to it do not suffer any damage and you can safely connect your electronic devices to it.

At Bürklin Elektronik you will find an extensive selection of power strips

Bürklins range includes not only a number of different power socket strips from renowned manufacturers such as Brennenstuhl, but also power outlets in many different variants.  Please also refer to the category workplace equipment to find more equipment for your workplace. If you have any questions about our products, you can contact us by phone at +49 89 55875-230 or send an E-Mail to Info@buerklin.com. From Monday to Friday from 8:00 to 19:00 we are at your disposal.

  • 1(current)
  • 2
  • 3
357 Products found
  • 1(current)
  • 2
  • 3